Dear TI-Team,
I'm currently evaluating the PGA900 and I would like to ask some questions which I couldn't clarify via the data sheet.
1) Compatibility of external resistive bridge and analog front end
a. Which resistance range of the sensor element is supported by the PGA900? I a 3 kOhm bridge possible?
b. Which offset of the bridge signal is supported by the PGA? => e.g. a signal span of 50 mV and a negative offset of -30 mV, is this possible?
2) Temperature measurement via an external diode
a. In the data sheet there is temperature measurement via an external element mentioned but only with a thermistor (PTC is mentioned)
b. Is it possible to use a diode as a temperature sensor element and measuring the voltage drop over the diode (with a constant current, one terminal of the diode connected to ground as described on p. 35 in the data sheet)?
Best regards
Tobias