This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMT70EVM: LMT70EVM Windows did not recognize device

Part Number: LMT70EVM

Hello,

I've just installed the LMT70EVM Installer v1.4.0.0 (Rev. B) from TI website in my Windows 8.1 64 bits PC.

When I run the program, it says that"Auto Connection Failed! Check COM port number" in a pop-up window.

In the main window, there's a message saying "Connect Failed! Check hardware. Exiting...".

In Windows Devices Manager, it identifies the MSP430-USB Example, but says it's missing driver.

Cable seems OK, device is powered and both red and green leds are turned ON.

I did not find any other software to download or install in LMT70EVM page.

What am I missing? Do I need to install something more? Where can I find it?

Thanks.