Hi Michelle,
Could you tell us which section of the code in "high accuracy lab" set the boot and the image loading time of IWR1443boost (time for setting the hardware)? the first frame time now is around 310ms during the power on, the frame time is about 35ms with our chirp profile after the first frame time, we try to reduce the time for the first frame for our application
Thanks and best regards,