This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612: Temperature behaviour

Part Number: LDC1612


Hi,

can you comment on the temperature compensation of the LDC1612. Does the differential measurement method is expected to have problems in the temp range of -40/+85°C?  

Thanks

Fred

  • Hi Fred,

                    There should be no problem operating in that temperature range. Change in temperature changes the inductance resulting in a change in sensor frequency (fSensor). In differential configurations a reference has the capability to cancel out temperature changes and other environmental effects. For more information please refer to section 8.1.3 of the datasheet: www.ti.com/.../ldc1612.pdf. I hope this helps!

    Best Regards,

    Bala Ravi