Dear team,
My customer is looking for the amount of power that needs to dissipate at fully working with the AWR1243P device with the following settings:
* A duty cycle of 66% (and 100% if possible)
* ALL 3TX transmitting in parallel at full power, with phase shifters and attenuator
* ALL 4RX receiving in parallel,
* ADC speed at 37.5MSPS (real-mode)
* LVDS Data mode
* exciter on master chip working (need to know )
What is the expected power need to dissipate?
Can we dispate some power from the top of the chip (Platic case)?
Thanks in advance and regards,
Shai