This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Any software command to substitute NRST switch reset?

Part Number: IWR1443BOOST


Hello,

I am running the capture demo on IWR1443BOOST with SDK MMWAVE_SDK_01_01_00_02. I can trigger the capture through terminal, connect the board via CCS, save gDataCube to a file, and see the ADC and range data via capture_demo.m file in MATLAB. However, when I need to trigger the capture again (after disconnecting from CCS), I need to reset the board via pressing the NRST switch; otherwise, the next trigger gives 'Error -1".

Is there any way to use a software command as a substitute for the NRST hardware switch pressing?

Thanks,
Sanjib