Hello All,
My customer is developing 2-chip X1243 radar.
The customer has met issue at booting stage:
1. For the first boot SOP = "5" (1 0 1). There is no correct feedback during firmware flashing thru UARTп. The same situation as described here
http://e2e.ti.com/support/sensors/f/1023/t/713570
After UART Brake X1243 sends 0s. And after that X1243 sends received data back.
2. A strange behaviour VIN_13RF2 (Pins C2, D2). The voltage is rising to 1.8 В. VIN_13RF1 is OK.
The same situation at both chips. Independent voltage sources: TPS7A8801 * 2pcs
Best regards,
Dmitry