This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8241-CDK-EVM: Illumination board

Part Number: OPT8241-CDK-EVM

Hi. Can you please give me an idea of how easy it would be to detach the illumination board from the sensor board?

My plan is to change the illumination direction and the location of laser source, which will require separating the illumination board and the sensor board but connecting the two through about ~30cm wire.

Can you please also tell whether it might possible to change the diode to allow the illumination at a different wavelength?


Thank you in advance.