Other Parts Discussed in Thread: MMWAVE-SDK, IWR1642,
Hi,
I'm referring to this thread https://e2e.ti.com/support/sensors/f/1023/p/660937/2430814
Can I have access to this python script to decode the UART byte stream too?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm referring to this thread https://e2e.ti.com/support/sensors/f/1023/p/660937/2430814
Can I have access to this python script to decode the UART byte stream too?
Hi John, thanks for pointing me to the relevant thread.
Some questions about the structure i'm referring to at mmwave_sdk_02_00_00_04/packages/ti/demo/xwr16xx/mmw/docs/doxygen/html/index.html
Is this the correct document to refer to? I'm finding that the totalPacketLen (Total packet length including header in Bytes) does not match the bytes i receive.
is subFrameNumber always included in the header? so number of fields excluding the magic word is 8, not 7?
in mmw__output_8h_source.h, the enumeration values for message output are missing, what should the values be?
typedef enum MmwDemo_output_message_type_e { MMWDEMO_OUTPUT_MSG_DETECTED_POINTS = 1, MMWDEMO_OUTPUT_MSG_RANGE_PROFILE, MMWDEMO_OUTPUT_MSG_NOISE_PROFILE, MMWDEMO_OUTPUT_MSG_AZIMUT_STATIC_HEAT_MAP, MMWDEMO_OUTPUT_MSG_RANGE_DOPPLER_HEAT_MAP, MMWDEMO_OUTPUT_MSG_STATS, MMWDEMO_OUTPUT_MSG_MAX } MmwDemo_output_message_type;