Other Parts Discussed in Thread: IWR1443, MMWAVE-SDK
Hello All,
My customer has some concerns after using AWR1642.
He was present at mmwave seminar.
Customer is testing AWR1642, but this does not have a sleep function that greatly reduces the consumption (the ideal is to have a sleep mode with consumption much lower than 1mA or a function of switch-on much faster.
This is the biggest limit for customer right now.
May be IWR1443 can reduce consumption in a significant way?
These are the measurements customer found:
Total duration of start, setting and measurement of radar board: 440ms
There is a second time that could be associated with the actual measure, equal to 95ms.
So it may be that about 340ms of difference are just for the start and configuration of the system, and disappear in the presence of a sleep.
Any comments/advice here?
Many Thanks,
Antonio