Other Parts Discussed in Thread: LDC1614, LDC1101
I need to measure differential displacement as distance of 2 metal walls from two coils, either on X than Y axis (4coils as total)
1) Is the LDC1614 the correct choice for this purpose or is better use 4 separated LCD1101?
2) Is the firmware inside the microprocessor of the evaluation module available as open source in order to rearrange it as differential displacement sensor?
3) in order to get the best sensor displacement linearity, it is better use Rp measurement and than calculate the rate Rp/L , while the two characteristics has nearby the same behavior over Target distance/Sensor diameter?
Thanks of all,
Maurizio Liverani
stilsas@libero.it