Other Parts Discussed in Thread: OPT9221
In the process of trying to bring up the OPT-8241-cdk-evm, it seems that the laptop is having trouble initializing the eval board. The machine is a Win 7 machine with USB 2 ports. The voxel viewer downloaded and installed cleanly. The LEDs indicate the board powered up correctly. The Master LED is on and green. The Chipset LED is on and blue and the Status LED is on and red. The USB drivers auto-installed cleanly also. When I bring up the Voxel viewer, I get a Video Mode pop-up that says it "Failed to set frame rate as 30.00fps". When I bring up File->Select Depth Camera, it recognizes the camera is connected, however there is not video.
Suggestions?
BC