Hi,
a customer is using the AWR1243 with CSI2. The Data Flow document at
explains the data format for LVDS for both Non-interleaved mode as well as interleaved mode. For example for the interleaved mode the Figure 22 in the document shows how 8 CBUFF units are mapped to the 4 LVDS lanes.
Since the customer is using CSI2 instead of LVDS, we are looking for a mapping of CBUFF units to what appears on the CSI2 lanes if that is possible. Since CSI2 is a packet interface, and the customer has implemented a CSI2 receiver on an FPGA and data is being received, we would need to know how to interpret that data.
Could you help with that?
Thanks!
--Gunter