Hi
We want to care about implementation error of magnet.
So we are considering DRV5032DU (X2SON package) to detect magnet regardless poles.
It means detect magnet even if the pols is either N or S.
Magnet would be thin cylinder and surface of magnet is faced to IC with one side (N or S).
So one pole should be detected at once in the system.
To realize this requirement, is it possible to connect out1 and out2 together?
BestRegards