Hi team,
I am facing a problem with firmware load over SPI between different versions of AWR1243 devices. My problem is as below.
I power on the device, load the firmware and the config for the master then followed by add device and load firmware for slaves. I am always getting an error /hang during the firmware load of the slave.
I have tried increasing the timeout for the SPI/interrupt for every message to 5s. Still the error happens
This approach works superbly fine with my earlier version of the custom board, but doesnt work with the current version. (there is no hardware PCB change between the two versions of the Custom board).
My questions are as below:
1) I suspect that there are some minor changes related to hardware chip versions on my boards.I suspect this is related to the Bootloader as it might be expecting some process flow differently and I am doing differently in Sw (as per old version). Can anyone help us to confirm whether there are any changes in this regard between ES1.0, ES2.0 and ES3.0 for AWR1243?
Please note that the Custom Board is from my Customer and I don't have any information regarding which ES version is being used in old custom board and new custom board.
2) I am pretty sure that the current Custom board uses AWR1243P. Hence, My earlier question applies here again.
Is there any minor changes in Boot loader, that changes the firmware load approach between the devices AWR1243 and AWR1243P.
Any pointers on this issue will be really helpful.
Thanks in Advance,
Santhana Raj
PS: We are using 4 chip Cascaded mode of AWR1243.