Other Parts Discussed in Thread: TL071
Hello,
we need to acquire data from a 3-axis accelerometer and 3-axis angular rate sensor.
Each channel is a bridge, and we thought of using your PGA302 device, or a similar one.
However, our sensors need an excitation of 3mA (accelerometers) and 6mA (angular rate sensors), which is more than the 1mA stated in the PGA302 datasheet.
Also, we would like to read the data through a digital interface (SPI, I2C, etc.). Only if the digital interface is not fast enough, we would sample the DAC output of the device.
Since we need a sampling frequency of 20kHz (this is the bare minimum, a higher frequency would be preferable if possible), it seems like I2C is not fast enough (at least at a standard 100kHz speed).
Do you have other devices in the PGA302 family to meet our needs?
Or other devices for bridge acquisition?
Regards
P.S. The sensor we need to acquire is this: www.thp-systems.com/.../DTS-DatasheetDTS6DX-PRO_DSH-003.pdf