This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: Sensors forum

Part Number: TMP117
Other Parts Discussed in Thread: TCA9548A

Dear Technical support Team,

I'd like to use multiple TMP117 (Max 64) on I2C bus.

Is it possible to implement following configuration?

MSP430 has two I2C port.

【Case1】

Datasheet shows below. 

So I think following 64 TMP 117 configuration as slave is possible to use two TCA9548A , right?

■Total 64pcs

MSP430 I2C① →TCA9548A(8ch) → TMP117 x 4 pcs  / ch  x 8 ch (32pcs TMP117)

MSP430 I2C② →TCA9548A(8ch) → TMP117 x 4 pcs  / ch  x 8 ch (32pcs TMP117)

【Case②】

TMP117 has deivce id on register 0Fh and it shows x117(Hex).

Is it possible to use multiple TMP117 as slave  on single I2C bus below without TCA9548A?

MSP430 I2C →TMP117 x 117 pcs 

Best Regards,

ttd