This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004: FDC1004

Part Number: FDC1004

Hello,

I've currently implemented a liquid level sensor that should be located on a pipe. The level is read by FDC1004 IC following SNOA92 document. dimensions of the sensor are:

- Plastic Tape width: 25mm

- GND and LEVEL strips witdh: 3mm. Signals are connected respectivelly to ground and Ch1 (CIN1).

- RL and RE pads width: 3mm. Signals are connected respectivelly to Ch2 (CIN2) and Ch3 (CIN3).

- SHIELD strips width: 6mm. Signal is connected to SHLD1.

Channel Ch4 (CIN4) is left floating. Sensor length is 10 meters. signals are located on a face of the tape, whereas SHIELDS are located on the opposite face covering the signals.

Issue:

When I get the MEAS values (MEAS1 = Ch1-Ch4, MEAS2 = Ch2-Ch4, MEAS3 = Ch3-Ch4) I always obtain 0xFFFFFF00.

Questions:

- What are the best dimensions and clearance I should respect in order to deploy the pastic tape (i. e.: the base of my Sensor). In other hands are the chosen dimension suitable for the application?

- Is possible to use a sensor length of 10 meters?

- If NO, how can I get the maximum operating lenght?

- There are some improvements I should take into account in the software (gain, offset, and so on)?

- if YES, how can I proceed?

Many Thanks for your collaboration.