Other Parts Discussed in Thread: DCA1000EVM, UNIFLASH, IWR1443, AWR1642
Hello,
I am using IWR1443BOOST together with DCA1000EVM and mmWave Studio. The example script DataCaptureDemo_xWR.lua loads the firmware each time the script is executed.
I would like to put the firmware for mmWave Studio in the QSPI flash in the same way as the firmware that comes with the IWR1443BOOST board for the mmWave Demo Visualizer software.
I know the Uniflash tool and the changes for the SOP jumpers. The flash process itself runs without warnings or errors. However the board does not boot from the QSPI flash and shows a red error LED.
Is it possible to put the firmware that is delivered together with mmWave Studio to the flash memory?
Can anybody point we to documentation that I might not have seen (file conversion utility, flash instructions, ...)?
Best regards,
Matthias