This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: integrating with bst evm

Part Number: TDC1000-TDC7200EVM

hello, 

 I have integrated the tdc1000 tdc7200 evm with bst evm. When I enable the boost section, the excitation pulse seems to get distorted. I then removed the receive section capacitor(300pF) and then added a resistor of 1k. After which it seems to be working fine. May I know the reason for this? Is there anything that should be done so that I can use a capacitor in the receive section?Or should I use a different capacitor for this.