I got the DCA1000EVM yesterday and I followed the same procedures as mentioned in 'DCA1000EVM Quick Start Guide' to try its function.
1.Reset board
2.Connect RS232 Port
3.Run /mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\DataCaptureDemo_xWR.lua
However, there are some errors:
Ethernet Cable is disconnected Please Check...!
The file C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\..\PostProc\adc_data.bin is empty. Please capture more data.,
I am using the Win10 and the output logs are as followed, please give me some suggestions on how to solve this problem.
[19:47:43]
[19:47:43] ### Running Startup script: "C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\Startup.lua" ###
[19:48:34] TESTING = false
[19:48:34]
[19:48:34] ***Script completed successfully.***
[19:49:44] BSS FW Download Success
[19:50:06] MSS FW Download Success
[19:50:08] Power On Success
[19:50:08] MSS power up done async event received!
[19:50:10] BSS power up done async event received!
[19:50:11] RF Enable Success
[19:50:12] ChanNAdcConfig Success
[19:50:13] Regualar mode Cfg Success
[19:50:15] RF Init async event received!
[19:50:15] RfInit Success
[19:50:17] DataPathConfig Success
[19:50:18] LvdsClkConfig Success
[19:50:19] LVDSLaneConfig Success
[19:50:20] ProfileConfig Success
[19:50:21] ChirpConfig Success
[19:50:24] FrameConfig Success
[19:50:25] SelectCaptureDevice Success
[19:50:28] Ethernet Cable is disconnected Please check.....!!!
[19:50:28] CaptureCardConfig_EthInit Success
[19:50:29] CaptureCardConfig_Mode Success
[19:50:30] CaptureCardConfig_PacketDelay Success
[19:50:33] Frame start async event received!
[19:50:33] Frame End async event received!
[19:50:35] Please wait for a few seconds for Packet reorder utility processing .....!!!!
[19:50:51] Packet reorder utility processing done.....!!!!
[19:50:51] Please wait for a few seconds for matlab post processing .....!!!!
[19:50:51] [RadarAPI]: Error:
[19:50:51]
[19:50:51] ... MWMCR::EvaluateFunction error ...
[19:50:51] 23-Oct-2018 19:50:51: The file C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\..\PostProc\adc_data.bin is empty. Please capture more data.,1,
[19:50:51] Error in => process_adc_data.m at line 52.
[19:50:51]
[19:50:51] ... Matlab M-code Stack Trace ...
[19:50:51] at
[19:50:51] file C:\Users\ADMINI~1\AppData\Local\Temp\Administrator\mcrCache8.5.1\Matlab0\Logging\log_status.m, name log_status, line 32.
[19:50:51] at
[19:50:51] file C:\Users\ADMINI~1\AppData\Local\Temp\Administrator\mcrCache8.5.1\Matlab0\Processing_functions\read_adc_data.m, name read_adc_data, line 28.
[19:50:51] at
[19:50:51] file C:\Users\ADMINI~1\AppData\Local\Temp\Administrator\mcrCache8.5.1\Matlab0\MatlabPostPr\process_adc_data.m, name process_adc_data, line 52.
[19:50:51]
[19:50:51]
[19:50:51] Trace:
[19:50:51] 在 MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, Int32 numArgsOut, Int32 numArgsIn, MWArray[] argsIn)
[19:50:51] 在 MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(Int32 numArgsOut, String functionName, MWArray[] argsIn)
[19:50:51] 在 MatlabPostProcGui.MatlabPostProcGUIClass.process_adc_data(MWArray adc_file_name, MWArray force_cont_stream_mode)
[19:50:51] 在 AR1xController.frmAR1Main.iStartMtlabPostProc()
[19:51:01]
[19:51:01] ***Script completed successfully.***