Tool/software: TI C/C++ Compiler
Hello, TI!
I performed common offset calibration in our-self board base on our demo-board OPT8221.\
I have got these parameters: phase_corr_1 = -118, phase_corr_2 = 820.
I have question:
Do I write rightly to register negative value by I2C inteface (code fragment is below):
#define REG_5C 0x5C #define REG_58 0x58 #define REG_READ 192 #define REG_WRITE 193 //// some code unsigned char pocket_send[8]; unsigned char pocket_recv[6]; unsigned int len, gotLength; pocket_send[0] = REG_5C; pocket_send[1] = REG_WRITE; pocket_send[2] = 8; pocket_send[3] = 0; pocket_send[4] = 0x37; pocket_send[5] = 0; pocket_send[6] = 0; pocket_send[7] = 0; short temp; //temp = (phase_corr0<<4)&0xFFF0; temp = (phase_corr0 * 16)&0xFFF0; memcpy((char*)pocket_send + 5, &temp, 2); sendto(server_sock_cmd, pocket_send, sizeof (pocket_send), 0, (struct sockaddr *)&tof_adr_command, sizeof (tof_adr_command)); len = recvfrom(server_sock_cmd, pocket_recv, sizeof (pocket_recv), 0, (struct sockaddr *)&tof_adr_command, &gotLength); short temp_recv; memcpy(&temp_recv, (char*)pocket_recv + 3, 2); phase_corr0 = (temp_recv / 16); if(temp == temp_recv){ printf("Common Offset Calibration: phase_corr0 = %hi was successfully written to register\n", phase_corr0); }
here, I get -118 (for phase_corr_1), but I am not sure that register makes right interpretation of negative values.
2. What is the principal difference between phase_corr_x and hdr_phase_corr_x values and where/when first or second are used?