Other Parts Discussed in Thread: DCA1000EVM, , MMWAVE-STUDIO,
Dear Kyle,
Thank you very much for the very prompt and very detailed and elaborate guidance.
A few last queries in the same context so that I can make a better and informed decision:
1) I understand that you are suggesting AWR1642BOOST and DCA1000EVM based on my requirement that I mentioned.
Please advise/confirm that can I use/run mmwave Studio mmwave-Studio, mmwave-Demo-Visualizer and mmwave-Sensing-Estimator on xWR1642BOOST EVM (and I do not need DCA1000EVM for this purpose). Only AWR1642BOOST will serve the purpose. Please comment.
2) If I am not wrong, I understand that the ADC data from AWR1642BOOST EVM (and from AWR1642 device it self) is only available on 2 LVDS lanes. Am I right or not ? If not, then please advise that ADC data from the AWR1642 device and from AWR1642BOOST EVM is available in which other formats/prorocols for post processing on a Windows PC or some other Data Acquisition Card/Device ? (Suppose that I do not have DCA1000EVM).
3) A very basic question, but I still ask. I understand that the RF output (both in AWR1642 and in AWR1642BOST EVM), after the mixer, is available to the user, only after being digitized by the bulit-in ADC. The analog RF output signal is NOT directly available to the user. Please confirm.
4) What could be the possible usage or purpose of TI Launchpads (as AWR1642BOOST describes this feature) in my study on TI mmwve sensors. I intend to modify TI example codes or develop my own codes based on TI codes. Then I assume that I can upload those programs (e.g. bin files) through xWR1642BOOST EVM on the xWR1642 chip. I can then see the performance of my algorithms by acquiring and processing the LVDS raw ADC data and post processing it in PC, if needed. In such instance, I will not need TI Launchpads as I do not foresee usage of additional TI microcontrollers. Please comment if my understanding is right.
Thank you very much in advance.