Hello,
I am using a TDA2px( Master) to communicate with AWR1243( Slave) using FPD-Link connection. As AWR1243 supports only SPI communication and no I2C, I have used a SPI-I2C bridge SC18IS602B (same used by D3 for radar satellite configuration as mentioned in the original post) to convert the I2C Control to SPI Command for interfacing with radar sensor.
How should I connect the address pins A0, A1, A2 of the SPI-I2C bridge SC18IS602B? Should I connect them in pull up or pull down? As per the datasheet of SC18IS602B, the three pins are used by Master for addressing the slaves. In my application, the master would be the TDA2px and the slaves would be the radar sensors AWR1243. But I do not know what the address of the slaves 1243 are as I believe AWR1243 supports only SPI communication. Hence, I am confused on what address are they referring to in the datasheet?
I look forward to your reply. Thank you!
Best Regards,
Nishant