This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA411-Q1: The condition to cause "Tracking Loop Error"

Part Number: PGA411-Q1

Hello Resolver Sensor Team,

I got a question from my customer(Automotive Resolver).
PGA411 is RD Converter, which configured sin/con input.

If the rotation speed goes up immidiately, the RD converter cannot track the rotation speed, and cause "Tracking Loop Error".
The customer want to know the boundary of angular velocity.

Let's see the attached file showing example.

PGA411_Tracking Loop Error.pdf
If the rotation goes up from 1500rpm to 2000rpm -> No Loop Error.
If the rotation goes up from 1500rpm to 3000rpm -> No Loop Error.
If the rotation goes up from 1500rpm to 6000rpm -> Loop Error.

Just like above example, could you check the boundary rotation speed?

++++++++++++++
Regards,
Toshihisa Ishii in TIJ/west