This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/AWR1642: About Building Error issue

Part Number: AWR1642

Tool/software: TI C/C++ Compiler

Hi SIr 

We used mmwave_sdk_02_01_00_04 and import people counting project from mmwave_industrial_toolbox_2_5_2.

During image generation, we can build DSS successfully. But we met issue while building MSS. and below is the error message


'Building file: "../mss_main.c"'
'Invoking: ARM Compiler'
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/ti/workspace_mmWave/pplcount_16xx_mss" --include_path="C:/ti/mmwave_sdk_02_01_00_04" --include_path="C:/ti/mmwave_sdk_02_01_00_04/packages" --include_path="C:/ti/mmwave_industrial_toolbox_2_5_2/labs/lab0011-pplcount/lab0011_pplcount_pjt/radarDemo" --include_path="C:/ti/mmwave_industrial_toolbox_2_5_2/labs/lab0011-pplcount/lab0011_pplcount_pjt/radarDemo/chains/RadarReceiverPeopleCounting/mmw_PCDemo/gtrack" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR16XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_SIZE=0x40000 -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mss_main.d_raw" --cmd_file="configPkg/compiler.opt" "../mss_main.c"

>> Compilation failure
subdir_rules.mk:37: recipe for target 'mss_main.oer4f' failed
"../mss_main.c", line 407: warning #169-D: argument of type "int32_t *" is incompatible with parameter of type "rlCalibrationData_t *"
"../mss_main.c", line 407: error #167: too few arguments in function call
1 error detected in the compilation of "../mss_main.c".
gmake[1]: *** [mss_main.oer4f] Error 1
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
makefile:159: recipe for target 'all' failed

**** Build Finished ****

please advise and thanks

BR

Yimin