Reviewed materials on selection of Transducers for use with the TDC1000.
I am looking to select a transducer which will operation in the 1" to 10" distance range with the TDC1000.
If I could resolve 1mm would be desirable, but to achieve the distance mentioned above, willing to compromise.
I am trying to measure liquid height in a confined space, so beam diameter has to be narrow ( around 2.5" diameter and 8" tall.)
So the transducer will basically work through air and reflect off the liquid.
May have to seal the transducer, so this could be a consideration later down the road.
Can anyone recommend a transducer type, diameter, frequency, beam width, supplier?
Regards,
Thanks for any assistance.