Hello,
I have already asked related questions here.According to the recommendations, there has been some progress now.But I still have some problems.
Now when running the CANFD demo, the oscilloscope can measure the differential voltage waveform between CANH and CANL.As shown below:
Q1: Although there is an output waveform, once the host computer initializes PCAN-USB, the waveform disappears.
Q2: How do I calculate the parameters in the Bit rate Input box in the TI CAN Visualizer GUI? How to correspond to the parameters in the SDK code below?
/* Configuring 1Mbps and 5Mbps as nominal and data bit-rate respectively
Prop seg: 8
Ph seg 1: 6
Ph Seg2 : 5
Sync jump: 1
BRP(Baud rate Prescaler): 2
Nominal Bit rate = (40)/(((8+6+5)+1)*BRP) = 1Mhz
Timing Params for Data Bit rate:
Prop seg: 2
Ph seg 1: 2
Ph Seg2 : 3
Sync jump: 1
BRP(Baud rate Prescaler): 1
Nominal Bit rate = (40)/(((2+2+3)+1)*BRP) = 5Mhz
*/
Thanks,
eehzux