Other Parts Discussed in Thread: IWR1642, AWR1642
Hi,
I am trying flashed to run "lab0003_occupancy_detection" binary in IWR1642.
To configure the device using serial port I give following commands
mmwDemo:/>sensorStop Done mmwDemo:/>flushCfg Done mmwDemo:/>dfeDataOutputMode 1 Done mmwDemo:/>channelCfg 15 3 0 Done mmwDemo:/>adcCfg 2 1 Done mmwDemo:/>adcbufCfg -1 0 0 1 1
I get the acknowledgement up till "adcCfg" command.
As soon as I enter "adcbufCfg" command as shown above, the device hangs and doesn't respond.
Since I am using IWR1642 evm instead of AWR1642 evm.Please confirm If I can use AWR1642 binary in IWR1642 evm?
If yes, please suggest the method to resolve above issue.
Thanks in advance
Vikas.