Other Parts Discussed in Thread: PGA900,
Hello
Can the PGA900 reference designs used for the PGA 305?
Is there a reference design withjumper selectable 4-20mA or -010V output?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Harald,
The PGAxxxEVM-034 can accommodate either the PGA900 or the PGA305 and has jumper options for running the devices in either current or voltage mode. You could get the PGA305EVM-034 and samples of the PGA900. The PGA305 is socketed, so swapping out the chips is relatively easy to do.
Hello Tom
Thanks for your answer. But I asked for the reference design and not for the EVM. On the PGA900 website is a reference design for a device with 4-20 mA output. Can this be used 1:1 for the PGA305 too?
Single-Chip, loop-powered 4-20mA RTD Sensor Transmitter Reference Design
Best regards, Harald