Part Number: IWR1642BOOST
Other Parts Discussed in Thread: TIDEP-01000, IWR1642
Hello!
Can you point me to some information on how the additional azimuth resolution is calculated? I believe it is part of the Capon Beamforming but I'm having trouble working my way through the math around that. The device says it has a 120 degree field of view and when using 4Rx * 2Tx we get effectively 8 Rx.... which gives 120 / 8 and that describes that 15 degree azimuth resolution on the data sheet, right? But, the data in the point cloud is in increments of 1.875 degrees? The azimuth but doesn't seem to actually be accurate to that level of precision (for example, an item that is 10cm wide may be represented by SNR/doppler values spanning azimuth increments totaling 30cm across at the correct range). It is definitely more precise than 15 degrees so the data is helpful. Is there a way to get higher azimuth resolution?
Thanks
Tom