This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TDC1000-TDC7200EVM: Multiple errors building project TDC1000_TDC7200EVM

Part Number: TDC1000-TDC7200EVM

Tool/software: Code Composer Studio

- Windows 10

- CCS version 8.2.0.00007 

- Project out of the box.

- Long list of errors - see below some of them.

- TDC7200_basic_spi_readwrite & TDC1000_basic_spi_readwrite projects built without problems.

Thank you.


#1965 cannot open source file "descriptors.h" UsbMscScsi.c /TDC1000_TDC7200EVM/USB_API/USB_MSC_API line 50 C/C++ Problem
#1965 cannot open source file "descriptors.h" UsbMscStateMachine.c /TDC1000_TDC7200EVM/USB_API/USB_MSC_API line 48 C/C++ Problem
#1965 cannot open source file "descriptors.h" usb.c /TDC1000_TDC7200EVM/USB_API/USB_Common line 56 C/C++ Problem
#1965 cannot open source file "driverlib.h" usbEventHandling.c /TDC1000_TDC7200EVM/USB_app line 37 C/C++ Problem
#1965 cannot open source file "driverlib.h" usbdma.c /TDC1000_TDC7200EVM/USB_API/USB_Common line 42 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" TI_MSP430_spi_USCIB0_5xx.c /TDC1000_TDC7200EVM line 34 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" host_interface.c /TDC1000_TDC7200EVM line 37 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" main.c /TDC1000_TDC7200EVM line 40 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" msp430tdc_calculation.c /TDC1000_TDC7200EVM line 36 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" ports.c /TDC1000_TDC7200EVM line 34 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" tdc7200_calculation.c /TDC1000_TDC7200EVM line 36 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" timer_queue.c /TDC1000_TDC7200EVM line 37 C/C++ Problem
#1965 cannot open source file "TI_TDC1000.h" uart_commn.c /TDC1000_TDC7200EVM line 36 C/C++ Problem
#1965 cannot open source file "USB_API/USB_Common/device.h" UsbIsr.c /TDC1000_TDC7200EVM/USB_config line 39 C/C++ Problem
#1965 cannot open source file "USB_API/USB_Common/device.h" descriptors.c /TDC1000_TDC7200EVM/USB_config line 39 C/C++ Problem
#1965 cannot open source file "USB_API/USB_Common/device.h" usbConstructs.c /TDC1000_TDC7200EVM/USB_app line 35 C/C++ Problem
#20 identifier "MSC_MAX_LUN_NUMBER" is undefined UsbMscScsi.h /TDC1000_TDC7200EVM/USB_API/USB_MSC_API line 243 C/C++ Problem
gmake: *** [host_interface.obj] Error 1 TDC1000_TDC7200EVM C/C++ Problem
gmake: *** [main.obj] Error 1 TDC1000_TDC7200EVM C/C++ Problem
gmake: *** [msp430tdc_calculation.obj] Error 1 TDC1000_TDC7200EVM C/C++ Problem
gmake: *** [ports.obj] Error 1 TDC1000_TDC7200EVM C/C++ Problem

Some of the missing files are: descriptors.h, driverlib.h, cstring.h