Other Parts Discussed in Thread: IWR1443
Tool/software: Code Composer Studio
Hi
I would test CAN communication with IWR1443BOOST.
I read chapter 2.4.3 of IWR1443BOOST Evaluation Module mmWave Sensing Solution.
I have an IWR1443BOOST Rev.A. but I have PCB file of IWR1443BOOST Rev.B.
I have the CAN test source in this folder : C:\ti\mmwave_sdk_01_02_00_05\packages\ti\drivers\can\test
The doucument, IWR1443BOOST Evaluation Module mmWave Sensing Solution describes about Rev.A.
I have a question.
The CAN part between Rev.A and Rev.B is different.
Can the source be used to both Rev.A and Rev.B?
If the source cannot be used to Rev.A or Rev.B.
could you let me know the sample code to be able to use to both board.