This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: Raw data acquisition and range for amount of flow and TOF (ns) measurement by TDC1000-TDC7200EVM

Part Number: TDC1000-TDC7200EVM

Hello,

I want following information about the TDC1000-TDC7200EVM 

1) What is the min/max amount of flow it can measure?

2) what is the min/max TOF (ns) value it can measure?

3) How is the sensor mounting needed for the flow meter application?

4) Are APC Piezo sensors compatible with this module? 

Thanks.