Hi,
Please tell me how long the life of HDC2080 is.
For example, a SAW type humidity sensor has a lifetime of about one year,
Periodic replacement of the humidity sensor is required as a part with a lifetime.
HDC2080 Does the humidity sensor have a lifetime?
I would like to judge the life span by the deterioration of accuracy of the sensor.
Usage environment,
We are considering grounding in a sealed container filled with desiccant.
The ambient temperature is within the range of -10°C to + 60°C.
best regards
cafain