Other Parts Discussed in Thread: DCA1000EVM, , UNIFLASH, AWR1243, AWR1443BOOST, AWR1443
Using mmWave Studio 1.0.0.0 connected to a DCA1000EVM & AWR1243BOOST EVM, the following error is posted when performing a SPI Connect:
Status:Failed, Error Type: RESP TIMEOUT
I have erased the spi flash using UniFlash, but this did not fix the problem.
The SOP mode is 2 (SOP1 & 2 jumpers installed and 3 is out).
The system had functioned earlier, producing and displaying processed data. Upon one of the restarts, the SPI connect problem began as shown below: