This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: Antenna pattern for IWR1642

Part Number: IWR1642
Other Parts Discussed in Thread: , IWR6843, IWR6843ISK

Hi,

Though the antenna pattern is 120 degree in azimuth and 20 degree in elevation.

with IWR 1642 using any of 2Rx, 1Tx or 2Tx 4 Rx why it is not possible to get the range of object which is at, azimuth 0 degree and elevation 10 degree.

The mmwave demo is able to detect obly in azimuth of 120 degree. How do make it to work in elevation also.

Is is also fine if it gives range of this object. Since to get x,y,z direction extra Tx is required.

Range should be able to calculate using existing combination with iwr1642.

regards

Karthik s