This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: IWR1443boost ES3 board measurement time out error

Part Number: IWR1443BOOST

I import the project from TI attached folder to CCS, I am able to build both level_sense_demo and msp_level_sense_demo project successful (SDK3.0... latest version), and I flash Iwr1443boost board (ES3) with the file ti attached (prebuild), and flash the msp432 board with the new build msp_level_sense_demo.out, then attach two boards together with sop2 removed, start Tera Term, and take a single measurement, I get "measurement time out" error. the port is COM5 which is utility port, the baud rate is 115200. anyone know why, and what is the problem?

Thanks,