Other Parts Discussed in Thread: IWR1642
Tool/software: Code Composer Studio
Hello TI,
I am using PPLCount demo code for motion detection (SDK2.0, mmWave Industrial tool box 2.5.2 and IWR1642Boost EVM)
my application requirement:-
1.Fine Motion detection, It can be able to detect keyboard typing in 10/10 meter Hall
2. Range of IWR1642 is 10 meter with High accuracy detection
3.IWR1642 work Horizontally 120 deg and Vertically 60 deg
above mention points are possible to modify with pplcount demo and achieve the mention requirements ....?
I have go through pplcount customization guide and Programming Chirp Parameters in TI Radar Devices
i try to modify as per above mention doc but it not affect that much
1.trackingCfg 1 2 250 20 200 50 120
2.profileCfg 0 77 175 7 20 0 0 100 1 64 5333 0 0 30
3.SceneryParam -10 10 0.05 10
4.Radial velocity resolution(m/s): 0.04
there is any other reference for pplcount configuration modification ..?
Thanks,
Rahul