Hi,
This is related to the Error faced in running the occupancy detection GUI (od_demo.m). The error was " Not enough input arguments".
While putting some random values for the variables defined in the 1st line of the function i.e. ( comportSnum, comportCliNum, cliCfgFileName, polarPlotMode, decisionByMatlab ), I am not getting any error but the GUI displayed is blank with only two check boxes. I am attaching a screenshot of GUI on putting the values as (5,6,0,0,0).
What would be the correct values of the above variables to get the complete GUI displayed on system?
I am using the Automotive toolbox 2.0.0 with ES 1.0 EVM.
Thanks
- Nalini