In fact, if the ratio is the same (N/Rshunt) , the output error should be the same as the following calculation method, but I tried many groups of chips and found that the smaller Rshunt, the smaller the output error ,It
has little to do with proportions,why?
N=1000,Rshunt=1k:
8µT/(500µT/A) = 16mA (Primary current error)
This they calculates as 16mA/1000 = 16µA on compensation coil
With Rshunt = 1kΩ there is a 16mV at the input of the differential amplifier
Therefore after the differential amplifier you can get 64mV.
N=200,Rshunt=200:
The output should be consistent with the above theory,but actually the output error is smaller about 20mV ,I tested at least 10 pcs about drv421