This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-GASEVM: Transducer output pin does not output

Part Number: TDC1000-GASEVM


Hello Experts,

We purchased TDC1000-GASEVM and attempt to work it but a transducer output pin J1 and J2 of BSTEVM does not output any.

We are following the user's guide sniu026a.pdf.

  • Confirmed that TP2 of BSTEVM is 30V
  • 1V pulse is observed at TX1(J3 10 pin). 
  • Checked "TDC1000-HV Driver EN1 and EN2" on SETUP tab of GUI. 
  • Checked "TDC1000-HV Boost Power Enable EN"
  • Connected transducers on J1 and J2
  • JP1 is set to "HV"
  • VDD of U2 and U3( UCC27531DBVR) is 0V

Could you please advice what we are missing?

Regards,

Uchikoshi