Dear Technical Support Team
Do you have a comparison document between TMP117 and ADT7320?
Best Regards,
ttd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Technical Support Team
Do you have a comparison document between TMP117 and ADT7320?
Best Regards,
ttd
Hello ttd,
We do not have a document that compares the TMP117 and ADT7320, but here's a quick comparison on some of the specs between the two devices.
Property | TMP117 | ADT7320 |
Comm. Protocol | I2C | SPI |
Supply Range | 1.8V to 5.5V | 2.7V to 5.5V |
Operating Temperature TA | -55°C to 150°C | -40°C to 150°C |
Short range Accuracy (MAX) | ±0.1°C from -20°C to 50°C | ±0.2°C from -10°C to 85°C at 3.0V |
Whole Range Accuracy (MAX) | ±0.3°C from -55°C to 150°C | Unspecified, (TYP) is -0.85°C Typ at 150°C |
Resolution | 0.0078°C (16-bit) | 0.0078°C (16-bit) |
Programmable Interrupt | Yes | Yes |
Shutdown Current (MAX) | 500nA at 25°C | 15µA at 3.3V |
Curent - 1 Hz Sampling (TYP) | 15µA | 150µW at 3.3V |
Drift (TYP) | ±0.03°C | ±0.0073°C |
Both devices have: Programmable Interrupts, No calibration required, Shutdown Mode, and One-shot Conversions.
The TMP117 also has: Configurable averaging, Integrated EEPROM, and a Temperature Offset Register.
There are a lot of different conditions and requirements for these specifications, so the two devices do not compare easily. This information is just what I could pull quickly from the datasheet for the two parts. For a real comparison you will have to consult the datasheet of both devices, or if you have a specific spec you would like more information on I may be able to help with that.
Please let me know if you have any more questions.
Best Regards,
Brandon Fisher
just mention additionally
TMP117 is 6 pin 2x2mm package. ADT7320 is 16 pins 4x4mm package with the same thickness 0.8mm. It means the thermal mass is at least 4 times bigger.
PSRR is 0.006mC/V against 0.1C/V in ADT7320
There is no data what will be in ADT7320 a supply current (self-heating) when there will be 5MHz bypassing communication on SPI bus