I am planning to use the LMP91000 in an evaluation project with a 3 lead amperometric cell: an NO2 cell, requiring a negative bias.
I wanted to be able to have access to the precise voltage used for the internal zero at the trans-impedance amplifier and one way to do this seems to be to use bypass mode for INT_Z where I am providing the INT_Z from an external reference source.
If I then use the LMP91K in 3 lead mode, will the A1 amplifier and variable bias blocks still be in functional mode i.e. driving the external Vref plus/minus (0-24%) as bias to the CE terminal?