Part Number: HDC2010
Hello Support Team,
I am also useing right now 3 HDC2010 outside in a Housing, which allows a air circulation, but it is IP65.
I have a Problem with the Humidity. So we have at this time between 85% to 97% humidity. The Sensor sends me nearly all the time 99.9% humidity and sometimes it shut down for some hours.
The problem should be the dust and condensation.
What would be the best way to handle with this problem?
Should i start the Heater?
I have read in the forum, that i have to turn on the Heater as long as i do not receive the estimate value. But how do i know whats the erstimate value?
Thank you very much!