Other Parts Discussed in Thread: MMWAVE-SDK,
Tool/software: Code Composer Studio
Climbing the learning curve for a new development project, it seemed we would do best to start with the demo that comes with the mmwave SDK, the one that runs against the mmWave Demo Visualizer. But neither the SDK 2.1.0.4 and 3.0.0.8 demos seem to be available from the TI Resource Explorer site. The SDK subfolders have source code but none of the .cproject or .cssproject files we see in other projects.
It would be fastest if we can build our project on TI supplied code, and it seems better to start with the basic demo supplied with the SDK and add need functions, rather than a lab project where we would have to remove code.
1. Is there a Resource Explorer CCS project for the SDK 3.0 demo?
2. Is the demo in \ti\mmwave_sdk_03_00_00_08\packages\ti\demo\xwr68xx\mmw buildable using the files supplied in the SDK?
3. Would we have to build the project manually by creating the project and adding files in CCS? CCS V8 documentation seems limited and we haven't yet found detailed instructions for this for V7.
4. Or do you recommend a different or better way to get started?
Thanks
Dan Lewis