This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: Issue Editing Parameters for People Counting Demo

Part Number: IWR1642


I'm using my IWR1642 to do Texas Instrument's people counting demo. I'm trying to edit the allocation parameters for the demo (SNR Threshold, Velocity Threshold, etc.) but I can't figure out the best way to do it. I've tried opening the Matlab code for this demo (main_pplcount_viz.m) but I can't find in the code where to actually change the parameters, and I also can't even get the code to full run (I am unable to connect my device through the GUI created by Matlab). 

What is the easiest way to change the parameters, specifically the allocation parameters, for the people counting demo?