This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: About RS232

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: AWR1443,

Tool/software: Code Composer Studio

Hi

there is RS232 pins on AWR1443

How do I use RS232 pins ( Pin number N5, N6 ).

the sample code, water vs ground, uses Uart0 and Uart1 

Uart0 is command uart, Uart1 is logging uart.

I think they don't use RS232 Pins (N5, N6)

when I checked all pins of awr1443, pins about rs232 or uart are only N5 and N6.

What are the uart0 and uart1?

How do I use RS232 Pins ( N5 and N6)?

Is there a sample code for RS232 pins?

Regards.