Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi All,
I'm using the AWR1642 on one of the provided demos (at debug mode).
during the project stages ,i got the following message:
Error connecting to the target:
(Error -1180 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package 8.0.803.0)
explaination:
1.Flashed the 16xx debug bin (using the UNIFLASH when SOP0 && SOP@ are connected)
2.after succesful flashing-> removed the SOP2 and power cycled the device.
3.ccs-> compilation on dss and mss projects ->passed well.
4.Crearting new target configuration file, the TEST CONNECTION passed well.
5.after grouping ->the message appears when trying to "CONNECT TARGET"
Please assist.
Thank you
Gil