Hello,
I have successfully calibrated my sensor using a corner reflector. However, when I use the CLI generated compRangeBiasAndRxChanPhase command in a configuration file for the High Accuracy Lab, it either cannot load the file, or does so without accounting for the range bias. Is this because the High Accuracy mode is not expecting this configuration command? If so, is it just something that can simply be edited into the JavaScript source code for the visualizer?
Here is the configuration file I'm using for an object placed at approximately 0.6 meters away from the sensor:
RangeLimitCfg 2 1 0.1 1.0
Best,
Josh